1/15/2014 1:54 PM | |
Joined: 7/7/2010 Last visit: 4/24/2024 Posts: 14624 Rating: (2348)
|
Since you have not yet installed update 5 to V11 SP2, I would suggest you do that as it fixes many glitches/bugs and improves stability. What you may want is HSP 26 or 29 / 33 According to this pdf : http://support.automation.siemens.com/WW/view/en/54164095 HSP 11 is for V11 Professional. |
Last edited by: O_Moderator at: 1/16/2014 11:24 AMlink corrected science guy |
|
This contribution was helpful to1 thankful Users |
1/17/2014 7:16 AM | |
Posts: 10 Rating: (0) |
Hello Wizard, I think I meant wrong when I wrote H_11.Actualy is HSP_V11SP2_0026.Please look in the attachement. I will instal update 5 as you sayed to me and i hope it will work. Best regards. AttachmentPLC.zip (253 Downloads) |
1/17/2014 11:05 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hello cristiandoom, Here is a link how to install the Hardware Support Packages: how do you update the hardware catalog in STEP 7 (TIA Portal)? Best regards, Wizard |
1/19/2014 7:24 PM | |
Posts: 10 Rating: (0) |
Hello Wizard, I've done what you sayed to me.But still i can't start the plc. I plug in and it not starts. I used to work with s 7 200 before but i never had this kind of problemm. The plc not want to start.It standing in stop mode. That in way i think the software can not conect with,i think. There is another way to start it up? Or i have to make some settings in the software. I was looking on the internet on you tube and i saw ther taht it's very simple,the software recognize automaticaly the plcs. But i think those plcs are in the run mode. My plc not want to go in start mode. I'm disperate i don't know what to do enymore. Please tell me step by step what i have to do to solve this problemm. Here are few pictures. I wish you all the best. Cristiandoom
Attachmentplc.zip (232 Downloads) |
1/21/2014 9:34 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hello cristiandoom, |
1/25/2014 9:52 PM | |
Posts: 10 Rating: (0) |
Hi Wizard I wasn't home for few days.But i'm back and in this evening I've tried again to work with plc. I've readed all the posts from the link wich you send it to me but it was not very helpfull for me. Still can't conect. The protocol interface is PN/IE. How can i change it to TCP/IP? I'm thinking that is the problemm.I've enabled the internet protocol TCI/IP on my laptop but in the setings of the Tia Portal i can not find it. Here are some pictures attached. And about the ip i can not understand very well how it has to be. Best regards Cristiandoom.
Attachmentplc.zip (258 Downloads) |
Follow us on