2/20/2014 4:06 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172) |
There's only the product announcement yet: http://support.automation.siemens.com/WW/view/de/69065203 |
Have Fun! |
|
2/20/2014 4:14 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168) |
Hello Tom, Unfortunately not everybody can see that announcement Best regards, Wizard |
2/23/2014 11:40 AM | |
Joined: 5/4/2009 Last visit: 5/28/2024 Posts: 914 Rating: (40) |
So as a conclusion 1217 is not supported by V12 yet? |
Aim Higher |
|
2/23/2014 12:54 PM | |
Posts: 8946 Rating: (999) |
There is also no 1217 in actual catalog CA01. V13 will appear before you can buy a 1217, I think so. |
Follow us on