3/13/2014 8:09 AM | |
Posts: 45 Rating: (0) |
please see my attachment reagrding how am i checking the input
AttachmentSM1232 ANALOG OUTPUT PROBLEM.pdf (212 Downloads) |
3/13/2014 11:10 AM | |
Posts: 45 Rating: (0) |
i had created a new program , the analog outputvoltage all the channels to voltage, and checked but stil i m not getting anything, i changed the output module with a new one but still the same, is there anyother setting, can i troublehsoot the module in some way in the program everything shows ok and no error on the diagnostic page , i had also connected a 500 ohm resostor across that but still also nothing, is there any thing on the wiring , i had connect +24v to L and negative to m and earth to earth terminals in the program i m moving a value of 12000 to each othput channels, at the terminals nothing coming. i m very much worried . am using tia portal v11 sp2 some one pls help me on an urgent basis, plsss AttachmentTEST.zip (158 Downloads) |
4/1/2014 10:14 AM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating: (110) |
for all the users which are looking for the solution. Please check the following thread: problems with anlog output sm1232, Good luck Sabine |
Follow us on