11/17/2008 9:05 PM | |
Posts: 510 Rating: (117)
|
The XSub programs are stored in the memory after the end of the program. Refer to the SIMATIC 545/555/575 Programming Reference Manual, 505-8204-2. http://support.automation.siemens.com/US/view/en/17514825The TISOFT Manual, TS505-8101-7 describes the aux functions necessary to load/save and convert your XSUB programs. The XSUB is in binary format so unless you have the source it won’t do much good to save it. Here is the link for the TISOFT manual.http://support.automation.siemens.com/US/view/en/1937294I have attached a very old application note which was published to assist SIMATIC TI customers with connecting 505 PLCs to Siemens Operator Panels, Regards,billwest.
Attachmentapp_202.pdf (620 Downloads) |
11/22/2008 2:14 PM | |
Posts: 510 Rating: (117)
|
I searched through all of my old files and documents but could not find anything about HMI.REC and I don't remember anything about it. Bill |
7/30/2014 2:56 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question was split to MP377 communication with SIMATIC 505 PLC. Best regards O_Moderator |
Follow us on