9/19/2014 5:11 AM | |
Joined: 9/18/2012 Last visit: 8/26/2024 Posts: 3 Rating: (0) |
Hi all. I am also facing the problem to makeprogramming. Please help me with Answer. Manual of the TI505 (figure6-50) ts: @ k10 si: 2 td: v37 di: n = 1 Why @ k10 is WX1000? The actual contents of K10 and K11 are: K10 = 0900hex K11 = 03E7hex For example, What should I do if you want to V300 the indirect address? Thanks. Attachmentfigure6-50.pdf (659 Downloads) |
9/20/2014 9:29 AM | |
Joined: 9/18/2012 Last visit: 8/26/2024 Posts: 3 Rating: (0) |
Hi.all There was a description of the code in the manual. Thank you.
Attachmentcord.pdf (677 Downloads) |
Follow us on