9/13/2010 9:34 AM | |
Posts: 41 Rating: (3) |
Hi all, I have been using an S7-1200 along with the Wonderware DASSIDirect server to communicate with Wonderware Intouch. Everything is working smoothly, however if I try and access a memory bit in the DASSIDirect server it does not pick it up what so ever. For inputs and outputs I have simply been using what I used in the ladder program. Eg. I0.0, Q0.1, MW10 etc. For the memory bit I used something like M2.1 in my ladder but what I add M2.1 in Wonderware Client is has not status of value, almost like it doesn't exist. [schnippschnapp] second question is transferred to Another Problem with S7-1200 and DASSIDirect server. Thanks for any help in advance! |
Last edited by: O_Moderator at: 9/14/2010 8:34 AMsecond question splitted to new thread |
|
This contribution was helpful to1 thankful Users |
9/21/2010 11:25 AM | |
Posts: 41 Rating: (3) |
This problem has been solved in the other thread which the moderator split. Thanks! |
This contribution was helpful to1 thankful Users |
9/21/2011 7:30 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Attach here screenshots of your settings there. best regards, Hristo Mihalev |
9/21/2011 11:06 AM | |
Posts: 41 Rating: (3) |
I found the TopServer works very well with Intouch and the S7-1200. The DASSIDirect server seems to be quite slow no matter what I try
|
Follow us on