8/14/2015 7:26 AM | |
Posts: 24 Rating: (0) |
Dear Expert I have a very basic question.I have 1200 CPU and G120 drive,I have to take data from drive using profinet and send it using modbus TCP/IP protocol to thrid party controller.I am going to configure it as server ,As 1200 have only one profinet port , Is this configuration will work? ------------------------------------------------------------------------------------------ |
Last edited by: MUKUL NIKAM at: 8/14/2015 7:28:00 AMLast edited by: Min_Moderator at: 8/14/2015 9:59:01 AMNew subject after splitting |
|
8/14/2015 3:38 PM | |
Joined: 7/7/2010 Last visit: 9/23/2024 Posts: 15217 Rating: (2417)
|
A network switch between the PLC and the G120 drive will allow you to have more than one network device, like HMI and PG/PC as well as the 3rd party controller connected to the PLC. I hope this is the answer you need.
|
science guy |
|
This contribution was helpful to1 thankful Users |
Follow us on