11/20/2017 10:59 AM | |
Joined: 3/17/2013 Last visit: 12/25/2023 Posts: 480 Rating: (43) |
Hi Expert house, We are having GEN IV air cooled VFD with 9 cells w/o cell bypass 4.16 KV input, 100 Amps cell rating. Since last two years we received at least 4-5 time Cell DC Bus low warning. Each time we checked and found blown fuse. Strangely all are coming on TRAFO SECONDARY delta side phase A2, B2 and C2. cells. We checked the faulty cells with external VARIAC and found drawing abnormal current with a typical 5 % of rated voltage indicating cell internal Capacitors/semiconductor fault. Questions are 1. Is there any aging for these power cells even with INPUT MV ON always 2. We have total 3 air-cooled drives and occurring problem in one drive only? Any thing to cehck. 3. Why the cell faults occurring only on Phase L2.. Thanks N Vijay AttachmentEvent Log 11-14-2017 16-24.txt (641 Downloads) |
Follow us on