12/13/2017 8:23 PM | |
Joined: 3/14/2008 Last visit: 9/23/2024 Posts: 2096 Rating: (937)
|
Hi GeorgeKaim, You will need to have AS/OS engineering license on your ES in order to engineer with PCS7. PCS7 consists of several programs like SFC, CFC editors. You won't need a separate license for each program unlike traditional Step7. For PCS7 V8.1, you need the AS/OS engineering license at least. When downloading your program to your AS, you will need AS RT PO licenses according to the objects used in your program. See the following manual for more information and the licenses you will need: Licenses and configuration limits I read that you also have 7.1 licenses?? You have to make sure that you have licenses of the same PCS7 version. In order to use V8.1, you need to upgrade your existing V7.1 licenses.
|
Last edited by: Jen_Moderator at: 12/14/2017 9:21:26 AMInserted right link. If I could help you, you can use the RATE button. Thank you. |
|
Follow us on