1/15/2018 7:25 PM | |
Posts: 80 Rating: (2) |
Does the IoT support communicating via LoRaWAN or it is necessary an additional shield module? |
1/16/2018 8:45 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, to use LoRaWAN there is the need for an additional shield. There is a costumer who is using this an as I know they are using this shield to use the IOT as LoRa endpoint. I am not sure what you have to do exactly to get this shield running. We are in contact with the costumer who is using this and I think I can provide you more information about this next week. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/23/2018 11:55 AM | |
Posts: 80 Rating: (2) |
Hi bergmanu, Do you have some more information about this? It would be grateful |
2/26/2018 7:58 PM | |
Posts: 4 Rating: (0) |
We are waiting for this Example, Please try to give us something with LORA. |
5/3/2018 3:57 PM | |
Posts: 3 Rating: (1) |
Please see if my POST could answer your needs. FlexSensor from EXPEMB - LoRaWAN Shield for IOT2000 |
This contribution was helpful to1 thankful Users |
Follow us on