6/22/2018 1:26 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980) |
Hello, what you mean? Which Slot? Do you have a screen? Christoph |
6/22/2018 3:40 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello gdn; The part number you are showing is for a ET 200PRO CM I/Omodule; it does not come (but is included in) the GSD file of the ET 200PRO for Profinet IO. The GSD file is used to integrate the interface modules of the ET 200PRO on a Profinet network: IM 154-4 PN High Feature (6ES7154-4AB10-0A.B0), IM 154-3 PN High Feature (6ES7154-3AB00-0AB0) ET 200PRO Profinet GSDML file: https://support.industry.siemens.com/cs/ww/en/view/21915937 Manual: ET 200PRO distributed I/O system https://support.industry.siemens.com/cs/ww/en/view/21210852 Look up the manual above for more information. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on