6/21/2018 12:58 PM | |
Posts: 9 Rating: (0) |
Hello All, I am using the axis simulation script: AxisSimulationOnOff_V1_3_2. I've already tried to modify the provided script, but I couldn't find a possibility to access the ST program variables. Its only possible to modify configuration or system variables of TOs. I saw in the system variables of the axis the variable called: simulation. But it doesn't change when I run the simulation mode with the script. Why? Please give me an information which variable may I use in the ST program, that describes I am in simulation mode? Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_1069149 at: 6/21/2018 12:59:16 PMLast edited by: AutoGen_1069149 at: 6/21/2018 1:11:00 PMLast edited by: Jen_Moderator at: 6/22/2018 9:12:27 AMNew subject after splitting |
|
6/27/2018 6:34 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
and which error? sorry is not enough information in the post to get any help |
Follow us on