7/18/2018 1:39 PM | |
Joined: 3/3/2016 Last visit: 8/14/2024 Posts: 140 Rating: (0) |
AttachmentDesktop.zip (483 Downloads) |
7/19/2018 12:57 PM | |
Joined: 3/3/2016 Last visit: 8/14/2024 Posts: 140 Rating: (0) |
Hi! I have factory setting the PLC via SIMATIC MMC. Given below that step. 1.Power is OFF PLC & Insert MMC-2 MB 2.Power ON PLC 3.STOP & RUN LED is blinking,then STOP goes to stable. 4.Then Power OFF the PLC & Remove the MMC. 5.Now power ON PLC . Now PLC is factory reset mode. NOTE: In MMC should have given below the file.Otherwise PLC can not restted. 1. DataLogs 2.Recipes 3.SIMATIC.S7S 4.S7_JOB.S7S. Thanks for help. AttachmentDesktop.zip (495 Downloads) |
Follow us on