9/19/2018 5:58 PM | |
Posts: 2 Rating: (0) |
Dear Siemens Team, We are trying to install DIGSI_5_V07.80.08 trial version. On installation of prerequisite it stops and gives error. The error report is attached with the email. The error seems to come from installation of loopback drivers or service. Please kindly help us to resolve this issue. Your kind response will be highly appreciated. Thanks and Regards, Nikunj Patel
AttachmentDIGSI_V7.80_SetupBundle.txt (521 Downloads) |
12/28/2018 9:18 PM | |
Posts: 1 Rating: (0) |
Hello I have the same problem of Nikunj Patel, i can't install DIGSI 5 V07.80.08 in Windows 10 Pro 64bits. The installation process is canceled when it gets to the Status: "Installing Loopback Adapter" in Prerequisites. Best regards!
AttachmentDIGSI_V7.80_SetupBundle.txt (461 Downloads) |
4/12/2019 9:03 PM | |
Joined: 2/8/2019 Last visit: 7/11/2024 Posts: 2 Rating: (0) |
I have the same issue trying to install digsi 5 in windows 10 pro x64 |
7/16/2019 2:59 PM | |
Posts: 2 Rating: (0) |
I have the same problem when trying to install digsi 5 in windows 10 pro x64 |
2/15/2020 11:02 PM | |
Posts: 1 Rating: (0) |
Finally after two days i solved the problem for windows 10 64 bit you should fix mfcu.dll by installing Visual C++ Redistributable Packages for Visual Studio 2013https://www.microsoft.com/en-us/download/details.aspx?id=40784 then install and enjoy Best Regards |
This contribution was helpful to1 thankful Users |
Follow us on