11/22/2018 2:06 PM | |
Joined: 8/3/2009 Last visit: 4/18/2024 Posts: 12813 Rating: (1632)
|
Hello Kamy you can do it in two ways: 1.) you give the Name as A String Tag in your UDT or String Tag into the Faceplate with the Interface. Then you can use a parameter field inside the Text of the Textfield or Button.. 2.) you can use the Text Property of the Textfield as an Interface of the Faceplate. Then you can define the Name of the Motor outside on the Instance your faceplate as a constant. Both is quite easy to do Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on