1/22/2019 3:59 AM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201)
|
Can you make an example for only one output? |
1/22/2019 4:15 AM | |
Joined: 4/29/2016 Last visit: 6/17/2020 Posts: 17 Rating: (0) |
I don't have a Logo or the HMI with me right now, but here's the program for one station. I can look up the VM addresses for B001 and B005 when I get back to work tomorrow. In the application, I'd like for the values for B001 and B005 to be read from the HMI -- two variables on screen that will each apply to 20 stations. PDF attached. AttachmentChargerTable_R1.pdf (311 Downloads) |
1/22/2019 7:00 AM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33817 Rating: (4201)
|
Hello Dan Aspen, I once created a program proposal for you. Look, if this is in your sense. AttachmentTimervalue.zip (344 Downloads) |
Follow us on