5/7/2019 11:28 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi devilman1069, no, this is not possible. The internal analog inputs are only for voltage measurement. For thermocouple or RTD you need this modules: Signalmodules: SM 1231 AI 4 x 16Bit TC 6ES7231-5QD32-0XB0 SM 1231 AI 8 x 16 Bit TC 6ES7231-5QF32-0XB0 SM 1231 AI 4 x RTD x 16 Bit 6ES7231-5PD32-0XB0 SM 1231 AI 8 x RTD x 16 Bit 6ES7231-5PF32-0XB0 Signalboards: SB 1231 AI 1 x 16 Bit TC 6ES7231-5QA30-0XB0 SB 1231 AI 1 x 16 Bit RTD 6ES7231-5PA30-0XB0 hope this helps, regards, |
FCK WAR! |
|
5/8/2019 9:28 AM | |
Posts: 10 Rating: (0) |
Thank you very much for helping me clarify the doubt regarding this matter. I hear a lot about using Arduino to work together with PLC. would you mind telling me the possibilities of getting the Arduino sensor data to the PLC and displaying it on an HMI compatible with the PLC that i'm using for this project.
|
5/13/2019 10:42 AM | |
Posts: 10 Rating: (0) |
Hello Duris, Thank you very much for your valuable information on this regard. I did further research and with the help of certain people in this community managed to find out certain library and software (http://settimino.sourceforge.net/) which helps connect the arduino with S7 PLC im going to try using this method if i come across any queries i will post it here. Thank you again, cheers,
|
This contribution was helpful to1 thankful Users |
Follow us on