1/11/2021 2:58 PM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (586)
|
Hi, do you know this new application example? - but sorry at the moment only in German language available: Bibliotheken für Kommunikation für SIMATIC ControllerThe library for HTTP communication (LHTTP) enables data exchange between a SIMATIC S7-1200 / 1500 CPU via the integrated Ethernet interface with another device in the local network or with a web server in the Internet via HTTP or HTTPS. Regards, Towome |
|
|
This contribution was helpful to4 thankful Users |
1/17/2021 5:22 PM | |
Joined: 12/18/2019 Last visit: 9/17/2024 Posts: 5 Rating: (2) |
Hi I think the LHTTP library works with 1200 from firmware v4.4 |
This contribution was helpful to4 thankful Users |
Follow us on