7/7/2020 6:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Please follow this link, enter motor article number & serial nmber, appropriate spares list will be displayed & you can get the desired one. You may refer attached sheet for information. HTH |
7/7/2020 12:24 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Dear Technology Team, thank you! |
7/7/2020 12:29 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, Is this motor connected with Siemens 611 series drive? What type of motor connector is i.e. is it full thread with union nut or speed connect or with external full thread? Your motor connector size is 0.5. However please find below here with article numbers of three types of connectors (for cable to be connected at motor end) Depending upon motor side male connector select matching connector from below list. . 6FX2003-0SU07 power connector with union nut full thread. 6FX2003-0LU50 power connector with union nut speed connect 6FX2003-0SA07 power connector with external full thread HTH |
This contribution was helpful to1 thankful Users |
Follow us on