7/25/2018 2:36 PM | |
Posts: 91 Rating: (1) |
Hi All, I was commissioning an 840D sl system with HSD spindle, 1Vpp sin/cos encoder feedback controlling by S120 drive. After configuring the spindle, I run it through starter it was working fine. Using the IBN tool I write the axis parameters and configured 5th axis as a spindle. But while I am running the spindle I am getting 25030 error. As per the help, it says to change 32110 MA_ENC_FEEDBACK_POL. I have tried to set 1,0,-1 But error remains same. we tried to compare the encoder direction using the starter and axis Diagnosis it showing the same direction. Even we tried the reversed motor rotation direction but still its same. IF we make the number of Encoder para : 0 then everything works fine. What can be the reason? have anyone face the same issue? AttachmentNC_25_7_2018.zip (270 Downloads) |
Last edited by: mehar at: 7/25/2018 2:37:13 PM |
|
7/25/2018 2:37 PM | |
Posts: 91 Rating: (1) |
Here i am attaching My starter backup
Attachmentdrive_backup_starter.zip (215 Downloads) |
Follow us on