9/25/2019 11:01 AM | |
Joined: 1/9/2019 Last visit: 8/20/2024 Posts: 87 Rating: (10) |
hi, I have SIMOREG 6RA70 drive operating in terminal mode running a dc motor with 1500 RPM nominal speed, with speed feedback of tacho, I wanted to lower the speed without changing my setpoint for example if my analog input is 5v my speed should be about 750 RPM but now if I give it 5v I want my speed to be 500 RPM which parameter should I cahnge? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/25/2019 12:54:18New subject after splitting Last edited by: The Helping Hand at: 09/25/2019 13:05:15New subject after splitting Last edited by: The Helping Hand at: 09/25/2019 13:05:51 |
|
Follow us on