4/13/2011 1:43 AM | |
Posts: 17 Rating: (0) |
Hello, i use wincc and i have some structure tags for my analog inputs. The format of the structure tags is TAG.value,TAG.RangeLow,TAG.RangeHigh,TAG.Filter,TAG.Alarm. I did a big mistake because i did not know and i create 4 tags andi named them for example test.value,test.RangeLow etc. Now i am trying to erase them but i get an error message like the one i attach. The point is that there is no associate structure tag...What can i do? Splitted form Deleting of structure/tag generated by AS-OS tool. |
Last edited by: O_Moderator at: 4/13/2011 9:18 AMnew subject after splitting |
|
4/13/2011 12:45 PM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
If you have SmartTools installed from the original CD, you can also use the Configuration Tool to update, edit, delete structure tags in Excel. |
B r g d s , |
|
4/14/2011 8:11 AM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
Like I said before, check with Configuration Tool to see possible leftovers in tags/structure tags |
B r g d s , |
|
4/15/2011 9:12 AM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
I was able to reproduce your problem. I had a Structure Tag in which I renamed 1 element by using the Configuration Tool. Afterwards, in WinCC Explorer I noticed that the Structure Tag was indeed changed by the tags created with that Structure Tag type, were not update and when trying to delete those tags, I got the same error message. The way to solve this was to rename that Structure Tag element to the old name with Configuration Tool again and then you can delete the tag. I think the tags you want to delete are somehow still linked with a Structure Tag element that doesn't exist (anymore). |
B r g d s , |
|
Follow us on