6/3/2021 11:34 AM | |
Joined: 5/25/2020 Last visit: 5/23/2023 Posts: 1 Rating: (0) |
I'm using Operate V4.94 and I have the same issue. I noticed that when you open Visual Studio from operate or by creating a shortcut with
I'm starting operate from my code after declaring these environment variables. I tried accessing to SALAL with DataSVC, but I was only able to read 16 of 100 messages and I was only able to get the message number, not the string content the parameter manual states that "The module SALA only contains the alarms that are generated in the NCK. It contains neither PLC nor HMI alarms. In order to read all alarms, the OEM-HMI user should use the alarm server functions and not read the SALA module directly." And I need the PLC and HMI alarms too, so I suppose that SALAL access is out of question too. |
Last edited by: Jen_Moderator at: 06/04/2021 10:02:58Optimized link. |
|
Follow us on