9/7/2014 11:22 AM | |
Joined: 9/14/2011 Last visit: 8/18/2020 Posts: 54 Rating:
|
Dear bg2492 I have gone through some manuals and yes I should go with the storage option also I have storage license on both the servers 1 & 2. But I tried to configure it but it is not working since the system is existing. Could you please advice me,some steps or the points which I should keep in mind to redfine the storage settings. my .DB file in both servers is already 5 GB now Please advice me. Thanks Raheel |
9/7/2014 3:08 PM | |
Joined: 5/16/2014 Last visit: 3/1/2021 Posts: 6586 Rating:
|
Hello Rahel, the configuration of Storage is somewhat strange, many customers had have problems with it in past. What is your target device for archiving (optical or JAZ or other HD on the same PC or share in network ? If you use a HD in the same PC, you should create a folder ("Archive") and create a share. Then use the share with UNC-name (i.e. \\COMPUTER\Archive) but not directly the local drive (i.e. D:\Archive) for the archivingdrive. Do never activate "Diskmonitoring", use only the "Repetition" with "Swap" for Alarmlogging and Taglogging. Report is usually no needed, there are no report data in the runtimedatabase. If the plant was running some years and the runtimedatabase is 5 GB, you have to archive a lot of data. Therefore you should set for "Data older then" a higher number of weeks (i.e. 500) and degrease this value after every succesfull archiving step by step. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
9/8/2014 11:54 AM | |
Joined: 9/14/2011 Last visit: 8/18/2020 Posts: 54 Rating:
|
Dear bg2492 Thanks for the valuable information you provided. In my case I am swapping the data to a Drive on the PC itself. In my case the existing folder is named as "BACKUP" I shared that folder and started doing "Swap manually". I can see something is updated in the folder but how I can open and see the privious alarms, do I need to import it? I can see in my BACKUP folder alarm.csv file is 0KB!!! But I got some Reports.EMF and Tag files. Thanks Raheel |
9/9/2014 12:51 PM | |
Joined: 9/14/2011 Last visit: 8/18/2020 Posts: 54 Rating:
|
Thanks bg2492 I will check and get back to you. regards Rahil |
9/21/2014 1:55 PM | |
Joined: 9/14/2011 Last visit: 8/18/2020 Posts: 54 Rating:
|
Dear bg2492 I did the changes as you instructed and I got 3 GB of data in the Archiv folder but still my "Project"RT.DB file is of the same size and this is making my hard disk even full in size. Is there any option where I can minimize the RT.DB file size after archiving it. AlsoI have connected a network hard disk of size 3TB, can I create a folder directly on the Hard disk and archive on it from both server 1 and server 2. Please advise. Thanks Raheel |
9/27/2014 11:22 PM | |
Joined: 9/14/2011 Last visit: 8/18/2020 Posts: 54 Rating:
|
Thanks bg2492 I will check and come back to you. Best regards Raheel |
Follow us on