7/3/2020 11:50 AM | |
Joined: 9/23/2005 Last visit: 4/25/2024 Posts: 4522 Rating: (698) |
First - that we need to answer questions without guessing. Second - one picture is worth of thousand words, show a screen shot of the code with all crucial details. |
Regards, |
|
7/3/2020 1:21 PM | |
Joined: 4/7/2012 Last visit: 4/9/2024 Posts: 112 Rating: (3) |
ok. I've various profinet device , than from slot 7 I can have the slot occupied of free . The copying of Extended I/O will be selected via software, and I would like to control if it is present or not. the problem is that I set to access E1012 ... and I don't get any error from the BLKMOV operation. (RETVAL = 0) |
Follow us on