10/17/2017 1:05 AM | |
Joined: 7/2/2016 Last visit: 12/11/2023 Posts: 115 Rating: (29) |
Hello Khanzada0786, the number max of I/O per CPU in 1200 line are: CPU - MAX DIGITAL - MAX ANALOG 1211C - 18 - 4 1212C - 86 - 20 1214C - 288 - 68 1215C - 288 - 68 1217C - 288 - 68 attached CPU specs compare Best Regards, DINIZ --- if it was helpful please rate the post.
AttachmentS7-1200 CPUs COMPARE.pdf (255 Downloads) |
hope this help, if it was helpful please rate the post! |
|
This contribution was helpful to2 thankful Users |
Follow us on