5/17/2020 11:00 AM | |
Posts: 1 Rating: (0) |
hi to everyone im a student and I really need logo8.2 comfort to do my exercises, but the problem is I can not install and use logo on may Mac OS Catalina 10.15.4 . can someone help explain me how can I do it ? or al list some online page to do my exercises ,I'm going to finish the school really soon and the professor just force us to make these ^homework^and send it to him . so something I can do ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/18/2020 10:51:01New subject after splitting |
|
5/19/2020 8:02 AM | |
Joined: 2/20/2014 Last visit: 9/17/2024 Posts: 396 Rating: (38) |
What type of "homework" are you referring to? Do you need to download the program that you write direct to hardware (LOGO! 8.2)?
|
5/19/2020 8:59 AM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33837 Rating: (4205)
|
@RKBIS, the topic starter can't install LSC V8.2 on his PC with the MAC OS Catalina. That is his problem... |
3/22/2021 1:44 PM | |
Posts: 1 Rating: (0) |
I'm using Big Sur, and when trying to install Logo. I only find upgrades, nowhere the full package. Any suggestions? |
Follow us on