12/6/2019 6:33 PM | |
Posts: 3 Rating: (0) |
Hi Everyone, I've got a D410-DP device (6AU1410-0AA00-0AA0) ,a CF card (6AU1400-2PA00-0AA0) and Siomoution Scout v5.2. When i'm trying to go online with the target system, i can only connect to D410 device but not to sinamics integrated, whitch is in D410 device. I tried to connect with D410 using fully new project, where D410 is the only inserted device. I tried to connect with working project, every time i firstly download the HW Config but result was the same: no connection with sinamics integrated. I droped the project 4 u. Help me pls! Looking for your reply. AttachmentLine14.zip (165 Downloads) |
Last edited by: N1kh!N at: 12/06/2019 18:36:24 |
|
This contribution was helpful to1 thankful Users |
12/6/2019 10:47 PM | |
Posts: 13 Rating: (0) |
It happened with me once. i have changed CF CARD. |
Follow us on