2/7/2017 2:24 PM | |
Posts: 9 Rating: (0) |
Hi Everybody! I'm trying to communicate S7-400 (CPU412-5H PN/DP) and S7-1200 (CPU1214C DC/DC/DC) using GET and PUT functions. I wrote the same functions for both of them. but I get error 1 in S7-400 and nothing transmitted. I also read manuals and forum conversations but I can't find where the problem is. I used SIMATIC S7-v5.5 for CPU400 and TIA Portal v13 for S7-1200. I created DB for both and addressed them. I used IP address 192.168.0.1 for CPU400 and 192.168.0.2 for CPU1200. I also enabled PUT/GET permition connection in S7-1200. I used the same ID address for CPUs. I also attached pictures. Thanks in advance ------------------------------------------------------------------------------------------ AttachmentS7-communication.zip (1468 Downloads) |
Last edited by: Min_Moderator at: 2/8/2017 11:45:06 AMNew subject after splitting |
|
2/12/2017 5:36 AM | |
Posts: 9 Rating: (0) |
Hi everybody Problem solved. I replaced FB14 and FB15 with SFB14 and SFB15 then everything went well, so I can send and receive data from s7-v5.5. Thanks |
7/21/2020 8:23 PM | |
Joined: 9/3/2014 Last visit: 9/10/2024 Posts: 9 Rating: (0) |
Dear Zahra_Kh, Will you please share, how did you implement communication between S7400H and S71200? |
Follow us on