8/26/2010 2:09 PM | |
Posts: 6 Rating: (1) |
I've tried to establish connection between two PLC. They were named by me PLC_1 and PLC_3. I'd like to check if the connection being established on the output "DONE" of function TCON on the PLC_1, unfortunately this "DONE" status is always and only set on the output of TCON function located onto PLC_3, regardless of the "Establish active connection" is set to PLC_1 or PLC_3. How to achieve the connection status "1"at the "DONE" output of TCON onto PLC_1 ? Please look at the attached printscreens. rumcajs Attachmentprintscreens.zip (857 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on