2/23/2017 5:45 PM | |
Joined: 1/6/2009 Last visit: 4/12/2024 Posts: 132 Rating: (2) |
Here is the logs files of winCC. If somebody can help me I will apreciate. Thank you. AttachmentLogs.zip (275 Downloads) |
6/17/2017 10:03 AM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Dear Thomas, thank you for the reply. In my case communication is working/established ok, Inbetween getting this communication error-that too not very frequent. There is 2 PLC connected to SCADA PC via D-Link switch. PLC is having fw of v4.1. As per the observation, even communication is not there, could ping ip address of the PLC from PC attaching the diagnose entry related to communication from wincc diagnose folder. Attachmentcommn.zip (248 Downloads) |
|
|
Follow us on