12/9/2020 11:06 AM | |
Joined: 6/24/2019 Last visit: 9/4/2023 Posts: 19 Rating: (0) |
there is a password but I have not configured |
12/14/2020 8:45 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello hichemaip19, do you user WinCC V7.5 or WinCC V7.5 with SP1 ? WinCC V7.5 is only released for using with S7-PLCSIM V15.0 WinCC V7.5 with SP1 is released for using with S7-PLCSIM V15.0, see compatibility tool https://support.industry.siemens.com/kompatool/pages/main/index.jsf?sitc=wwdfi10002
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
12/16/2020 2:22 PM | |
Joined: 6/24/2019 Last visit: 9/4/2023 Posts: 19 Rating: (0) |
on another pc i followed the siemens manual step he walked the first time |
12/21/2020 8:14 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41)
|
Hi, can you ping the CPU? B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on