9/12/2019 6:44 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello akbar; It is the IO controller that is charged with setting the IO device's Profinet address, once the IO controller has been configured with its IP address and Profinet name. Assigning names and addresses in PROFINET IO https://support.industry.siemens.com/cs/ww/en/view/19549525 After the IM 153-4 has been inserted in the Profinet network configuration, and once the IO controller has been restarted, it will receive its IP address from the controller; you also have to configure its Profinet name at this point. For more detailed information, download the pdf file "Automatic commissioning of a PROFINET IO system" from this link: https://support.industry.siemens.com/cs/ww/en/view/36741408 Hope this helps, Daniel Chartier |
9/14/2019 7:01 AM | |
Joined: 6/14/2015 Last visit: 3/26/2024 Posts: 236 Rating: (1) |
Thanks so much. but your answer is not very clear. I don't understand what should I do. |
Follow us on