12/31/2020 9:42 AM | |
Posts: 4 Rating: (0) |
Hello,
Which device do you use? I have magnetic pick up as well. It gives 1072 hz when reaches the highest rpm. But I cannot read it on plc. I looked for some circuit to convert hz to square pulse. But I am not sure whether they work accuretly or not. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 01/04/2021 09:23:12New subject after splitting; instert quote |
|
1/27/2021 1:20 PM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello Saktas, in the internet is an application example which presents different possible applications for high-speed counters (HSC) of an S7-1200. This could be useful for you. S7-1200: Application Examples for High-Speed Counters (HSC) With best regards |