2/9/2020 5:26 PM | |
Joined: 12/16/2019 Last visit: 10/24/2023 Posts: 9 Rating: (0) |
Hello, I'm struggling with the same issue as this topic on the forum: Connections modbus tcp - one client(s7-300) and two server device But I have some questions how to set this up. I'm working in STL and working with a CPU315-2DP V2.0 and CP343- Lean V2.0 a) How do I set up the second device in NetPro, Connect to same Ethernet network probably, but where I have to change de connection ID from 1 to 2 for the second device? b) How do I configure this in OB100? Copy DB100 to DB101 or modify OB100? How do I do this? c) How do I configure this in OB1? Who can help me with this? Best regards. |
2/12/2020 8:46 AM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (124)
|
Yes, and now you must insert 2 active TCP connections... |
2/24/2020 8:51 AM | |
Joined: 12/16/2019 Last visit: 10/24/2023 Posts: 9 Rating: (0) |
and here the project archive
AttachmentModbus_test_V3.07.zip (500 Downloads) |
Follow us on