10/3/2019 4:21 AM | |
Posts: 2 Rating: (0) |
Greetings, 1. I'm using CP1243-7 LTE with Singapore or any foreign sim card at Malaysia. May I know that, if this module can support roaming service or not? 2. Is there anyone has used before STC (Saudi) sim card with CP1243-7 LTE GSM module at Saudi? If yes, can i know what are the configurations you did to send out the SMS? Im already configure the module as per stated on TIA portal, but still couldn't send SMS from the device by using STC sim card. When i use the same program with Malaysian sim card, I could send out the SMS. I don't know whether there is any additional setting on program. Please find the attached program, Thanks. ------------------------------------------------------------------------------------------ AttachmentGSM_Siemens_LTE_27_09_19.zip (40 Downloads) |
Last edited by: The Helping Hand at: 10/04/2019 12:59:45New subject after splitting |
|
Follow us on