8/16/2009 11:04 AM | |
Posts: 212 Rating: (12) |
Hi Mankar, Named Connection is a type of configured connection. You need to create same via NetPro configuration. Stpe are below. 1. Open NetPro of your simatic Project. 2. Click on H-System AS. 3. On bottom part you will get a list where you can define the connection. 4. Click on the list to open a connection dialog box.(Creat Connection) 5. in this box you get a option to select the partner station in your case it will be Simatic PC station with CP 1613. 6. Select S7 Fault tollerant coneection and say apply ok. 7. If you have dual CP 1613 then select option "enable maximum redundancy". 8. Your Named connection is ready and same is available in WinCC under simatic protocol suite. Please find attached supporting document describing above steps. thanks, ABN AttachmentNetProConfig.pdf (718 Downloads) |
This contribution was helpful to1 thankful Users |
8/16/2009 12:30 PM | |
Posts: 37 Rating: (0) |
Hi... I attached my configuration in netpro.Is it correct? In pc station 1 i have to create a named connection in the name of s7connection_1 In pc station 2 i have to create a named connection in the name of s7connection_2 Iam going in right path? Attachmentconfig1.zip (300 Downloads) |
8/17/2009 6:05 AM | |
Posts: 212 Rating: (12) |
Yes, Its correct. |
8/20/2009 4:28 PM | |
Posts: 37 Rating: (0) |
Hi... I compiled the project there is no error.After creating XDB files i copied those files to my two os station.The problem is i am not able to communicate with the AS station.I attached some screen shots of my wincc configuration what may be the problem? And i also didn't know which name i have to give in logical device name? ( named connection -->system parameter-->logical device name) AttachmentNAMED CONNECTIONS.zip (375 Downloads) |
8/20/2009 5:46 PM | |
Posts: 37 Rating: (0) |
Hi... Attachmentnetpro.zip (225 Downloads) |
Follow us on