9/1/2017 3:21 AM | |
Posts: 305 Rating: (2) |
D425 and 1513 at PN , can you IRT connect ? Data via IO-device .... |
Last edited by: TechWing at: 9/1/2017 3:22:11 AM |
|
9/1/2017 8:02 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014)
|
yes |
9/1/2017 9:12 AM | |
Posts: 305 Rating: (2) |
in portal ,how can config it ? |
9/1/2017 9:22 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014)
|
give more informations! which TIA Version, Which PLC is io-device? |
9/1/2017 11:21 AM | |
Posts: 305 Rating: (2) |
PORTAL V13 , 1513 and SIMOTION D425-2 DP/PN |
9/1/2017 11:28 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014)
|
please answer the question correctly for a good help! |
9/1/2017 4:13 PM | |
Posts: 305 Rating: (2) |
D425-2 is IO-DEVICE,1513 is IO-CONTROL |
9/5/2017 6:02 AM | |
Posts: 305 Rating: (2) |
D425-2 is control ,and 1513 is IO-device ? how can do it ? |
Follow us on