5/25/2017 12:30 PM | |
Joined: 4/28/2015 Last visit: 7/14/2021 Posts: 3 Rating: (0) |
Dear Sir, Our VAP Partner purchased DESIGO X-Works Plus V6 and tried to installaton. But there is an error message is in bellow and I attached also. "The Network is not available. Do you want to resetablish the connection to the network?" They start installation as per release note in V6 program and required applications were installed already and there is not any problem in network including internet and mail. V6 program is V6.00.184_M300 and V6.00.342_ServicePack_M300. Could you check the error and advice to me? And is there any other installation manual of V6, I couldn't find in intranet and share folders. Regards, JiHooon Lee ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/26/2017 9:20:25 AMNew subject after splitting |
|
5/26/2017 9:26 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
The second thread with the subject Installation Error of DESIGO X-WORKS V6 is located within the conference Desigo™ Building Automation System. Best regards |
Follow us on