7/18/2006 12:32 PM | |
Posts: 1084 Rating: (72)
|
Hi, You say the picture are the same, does this mean you have only one picture or did you make a copy of that pictuer and renamed it? with regards, Ikkezelf |
10/11/2006 8:39 AM | |
Posts: 78 Rating: (3) |
[quote user="salma"]I do not use the OS Project Editor. Instead I manually create buttons and event scripts to load pictures into a PictureWindow. You can write the script using C or VBS, I think the OS Project Editor automatically creates the scripts in C. So you could look at the buttons you have and try manually adding / changing the code. However there might be an easier way to do this using the OS Project Editor. Does anyone know ?? Hi salma, after u posted this thread :"Everyone should read this ..." i'm afraid of asking question [:blush:][;)] anyway, we are appreciate u for answering the question [:)], thanx a lot I was trying to do it as u said, but i can't completely understand the c code that generates by OS-ProjectEditor, is there any reference for c-scripts that OS-PE generates?? or can u tell me more how can i do it manually?? i didn't find anything [:cry:] |
10/11/2006 10:20 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Hey no fair !! I want everyone to post questions here ... I just also want everyone to contribute to the answers [8)] Like I said I don't use the OS Project Editor, PCS7 or BPC so cannot help much with the scripts. Instead I can show you how to do it manually in WinCC. First thing to know is there is a wizard that writes thenavigation script for you. It's found under View -> Toolbars ->Dynamic Wizard -> Picture Functions tab -> "Picture Change in the Window". Once you have the basic script you can then modify it if necessary. I have put together some example screens. Just copy them into your GraCS folder, open the OVERVIEW.PDL picture and put it into Runtime. Any questions, just ask - I promise I don't bite [:)] BTW, I apologise in advance for the colour scheme used. I am completely useless at making pretty pictures / sexy graphics !! Attachmentpictures.zip (199 Downloads) |
Last edited by: salma at: 10/11/2006 10:46 AMoops, forgot the attachment again <img src="/forum/en/skins/emoticons/emotion-13.gif" alt="Rnf:lblSmileyTooltip_xxx" /> |
|
10/11/2006 12:24 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
[quote user="alfie"] 1: when i open ur screen, i encounter with "error while openning document" ... P.S. i'm using wincc6 sp 2 I am using SP4 which is why you cannot open the pictures. You cannot go back from SP4 to SP2 as explained here. Can anyone put together a quick SP2 example ?? I'm afraid I don't have a SP2 machine with me today. If no-one responds I should be able to do sotomorrow or Friday. [quote user="alfie"] 2: in teh picture function wizard, i cant see "Picture Change in the Window" i attached all that available there! Ah, of course you are using PCS7 and/or BPC. Use the wizard "Change picture in workspace" as I think it does the same thing. The wizard should look like the attached picture. |
10/14/2006 7:28 AM | |
Posts: 78 Rating: (3) |
Sorry guys, I didn't access to internet last 2 days, I'll check this out and share u my problems.[;)] thanx a lot |
Follow us on