1/14/2021 1:56 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
I would like to tell you that earlier we used Status Displays in Faceplates to visualize some information by changing the color or the small picture. And we took one StatusWord tag and parse it via the internal tags of the faceplate. Then I found a speed up solution. I deleted the internal tags and attached all the properties Index of the Status Displays to the external properties of the Faceplate. Thus I have to create many Dynamic Dialogs for a new instance of that Faceplate. But it is not a problem with the Visual Basic for Applications. And now I saw a nice solution for WinCC 7.5 — Animation and connection of the Structure tag. I remade all my Faceplate icons to this solution and what I saw: I am frustrated with those new functions. You may compare the last two versions of my Faceplate icons here: youtu.be/aqtowbBeIhg So I would say that in general the Dynamics Dialog works faster than Animation. |
This contribution was helpful to1 thankful Users |
1/14/2021 2:53 PM | |
Joined: 11/4/2011 Last visit: 12/8/2023 Posts: 253 Rating: (53) |
You are welcome. You may also want to read my answer here: https://support.industry.siemens.com/tf/ww/en/posts/wincc-v7-4-object-find-replace/253180/ And if you would ever try to create some tools in VBA then look at my list: |
Follow us on