8/22/2017 11:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello augt, Please check the PLC logic which will help you to find out the feed hold prolem. (510000 to 510015) |
2/15/2023 4:19 AM | |
Joined: 11/3/2022 Last visit: 9/2/2024 Posts: 4 Rating: (0) |
Bro where to check PLC logic , in the HMI or we need to connect to PC for verifying logic. |
2/19/2023 5:38 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, In Siemens user can not access PLC logic via HMI. User need to have Simatic Manager Step 7 v5.x with PG/PC + MPI cable. If user has hard copy of PLC logic, then referring it, user can check the PLC input, output, memory bit, words, data block etc. status on HMI in Diagnostic area. Hope this helps. |
Follow us on