9/13/2019 7:02 AM | |
Joined: 5/6/2010 Last visit: 4/24/2024 Posts: 1963 Rating: (272)
|
Hello, there is a support FAQ for this. the Entry ID is 109744698 - Which modules can you replace with S7-1500 running? Sorry, but actually is it not possible to insert links into a answer. Actually is the hot swapping not supported for the ET200MP (modules which you can use also in the rack) regards |
Last edited by: Jen_Moderator at: 09/13/2019 08:05:02Inserted link, because it's working for moderators. |
|
9/13/2019 2:23 PM | |
Posts: 8 Rating: (1) |
Thanks. But what about the modules on the same rack as the PLC? These are connected through C-Bus connectors. Is there anyway of hot swapping these? |
Follow us on