4/22/2020 12:51 PM | |
Posts: 36 Rating: (0) |
Hi! A have a very similar problem to this. I need to modify HMI program but the PLC program for that is very old and it seems to be a project for a SIMATIC manager. I already got some error msgs when I tried to open the project in SIMATIC manager. First of all a language problem, but It seems to be solver by added some extra language packs for the windows. So I decided to test the program with another project (pict 04) and it shows some missing software packages. Then I decided to check the target project required software packages and it shows many errors. And there is another project what looks different and may contain the same program but I don't know which program can open it. I attached the pictures. I am really new in using SIMATIC Manager. I appretiate any help! Lehel ------------------------------------------------------------------------------------------ AttachmentStep7_1-8.zip (63 Downloads) |
Last edited by: Jen_Moderator at: 04/23/2020 08:16:47New subject after splitting |
|
4/22/2020 12:56 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
Hello, you need software SIMOTION Scout.
Christoph |
This contribution was helpful to1 thankful Users |
4/22/2020 2:51 PM | |
Posts: 36 Rating: (0) |
Hi, I downloaded the SIMOTION SCOUT v5.2 SP1 and when I tried to install it an error occured. The current version is: V5.6+HF1 OEM2 Any suggestion? Regards, Lehel |
4/22/2020 2:53 PM | |
Posts: 36 Rating: (0) |
It should be in HF3 for this version? Regards, |
4/22/2020 3:00 PM | |
Posts: 36 Rating: (0) |
Hi, As I read somewhere the oem version may come with the STARTER. Okay I will take care of that. Regards, |
4/22/2020 3:10 PM | |
Posts: 36 Rating: (0) |
Hi, After I pressed "OK" on this message this came out and the setup exited. That shows my STARTER version is V5.3.0.1 Regards, |
4/24/2020 9:04 AM | |
Posts: 36 Rating: (0) |
Hi! Thank you, got it! Regards, Lehel |
Follow us on