8/2/2019 8:05 PM | |
Joined: 5/1/2018 Last visit: 8/10/2020 Posts: 2 Rating: (0) |
Hello this is the model of the sinumerik is 840c and the codes are: On the MMC the code is 8 On the NC-CPU appers two numbers first is 0 and then blink and apprears 8. The PLC-CPU the red led is blinking 11 times. The pictures I need to adjunt on PDF because I could reduce the size. I investigate in the manual and find that the code of the MMC is Code 8 is MMC powered without NC. But honestly I don´t know much about the Sinumerik. Thanks for the help. AttachmentPictures.pdf (90 Downloads) |
Follow us on