10/14/2019 5:07 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Petrov; You are attempting a connection over ISO_over_TCP, and for this you need to specify a partner PLC. PUT andf GET blocks use S7 communication connections. S7 communications ( for PUT/GET) use unilateral connections, no partner definition is required. I suggest you download the pdf provided by Ron7476 in the following discussion, it should guide you properly to setup the configuration and program blocks. Communication of S7-1200 With S7-300 via CPU 343-1 Lean Hope this helps, Daniel Chartier |
Follow us on