9/8/2020 10:52 PM | |
Joined: 9/27/2006 Last visit: 3/2/2021 Posts: 10452 Rating:
|
Hello Lanzx;
Hola Lanzx; El foro de Siemens atrae participantes de muchos países, y muchos no hablan español. Para facilitar nuestros intercambios, hemos elegido el inglés como idioma del foro. Haznos el favor de escribirnos en inglés a su proxima visita. Hello Lanzxñ The Siemens forum attacts participants from many countries, and many do not speak Spanish. To make our exchanges easier, we have chosen English as our forum language. Please write to us in English on your next visit. One issue: do you mean a SB 1232 module, 1 AQ, ±10 V or 0-20 mA, 6ES7232-4HA30-0XB0? Then have a look at this datasheet and connection diagram from the S7-1200 System manual: https://support.industry.siemens.com/cs/ww/en/view/109772940/108272746635 As stated, you cannot have a range of 0-10V, the only possible range is ±10V,; Check out if the suggestions from our friend O_Einstein in the following discussion can be of help: Problems with module SB 1232 AQ and PLC s7 1200 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/08/2020 22:53:16 |
|
Follow us on