4/18/2012 4:19 PM | |
Posts: 34 Rating: (3) |
**repost from different product conference** I'm working on a two axis project, I have two 1FK7060 motors on a double motor module. I've configured everything and and am able to take control of the both motors through the sinamics side and simotion side from the control panels. However when I give control to my program and go to move the motors I get fault 1910 and 1912. They are configured with the siemens telegram 105 message frame. I've gone through and checked all the parameters that the help topics from the error codes suggests. But I still can not find the problem. I've uploaded the fault logs in .zip format.I've included a few logs from different times I've encountered the errors. Also included is the diagnostic buffer from the D425. In the diagnostics buffer the events dated 4-13-12 are relevant the other fault logs uploaded. I really hope someone has an answer. =) I've already spent many hours trying to correct this problem. Also, I had worked with a D435 six axis system and had the same problem. We had a siemens rep at the site helping with some other issues and he noticed the fault 1910/1912 and clicked a few things changed some setting and suddenly it was gone. Unfortunetly, I did not pay attention nor did he tell me what he did. Thanks in advanced!! -Seb
Attachmentfault logs.zip (520 Downloads) |
7/6/2019 2:30 PM | |
Joined: 6/27/2011 Last visit: 9/21/2024 Posts: 4 Rating: (0) |
Could u please tell me how you solved this issue |
7/6/2019 2:34 PM | |
Joined: 6/27/2011 Last visit: 9/21/2024 Posts: 4 Rating: (0) |
Please explain how to do this....I am not familiar with simotion could you please help me out |
12/11/2023 7:49 AM | |
Joined: 12/1/2023 Last visit: 6/27/2024 Posts: 1 Rating: (0) |
Que tal christophD algun medio para contactarte por favor |
12/11/2023 12:19 PM | |
Joined: 8/21/2014 Last visit: 9/23/2024 Posts: 1024 Rating: (14) |
Hello chaco10 Please try to discuss your question in English language. This is an internationalcommunityand we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
|
My Forum is the place to personalize your profile, |
|
Follow us on