7/4/2019 10:10 AM | |
Joined: 12/25/2018 Last visit: 9/17/2024 Posts: 76 Rating: (0) |
we have a cnc vertical lathe machine with sinumerik 840d control, when the process for tool change is requested the machine is positioning the X axis in tool magazine area and unclamp the tool holder. the next step is supposed to go the -217 mm down to pick up the tool. at this moment the screen shows Dis. to. go -217 mm and there no movement on axis. when we check the condition of the program it is in wait stage and shows feed rate is 0. the knob for the selector is at 120%. can anybody help us to find what is the problem. More information can be provided up on request. Thanks in advance. Attachmentfile.pdf (49 Downloads) |
Last edited by: shafid at: 07/04/2019 10:11:08Last edited by: shafid at: 07/04/2019 19:28:53Last edited by: shafid at: 07/04/2019 19:36:39 |
|
Follow us on