7/18/2006 2:31 PM | |
Posts: 8 Rating: (0) |
Hi, i just started useing WinCC, im a student working at Siemens in denmark, and read a little about the program but already doing some "programs". Here is my question (maybe more will come ;)) Picture to help (sorry about the quality) http://peecee.dk/?id=47885 first a little info, when i "push" up the "wincc slider control(4)" the "wincc gauge control(3)" follows it, when i press "STOP(1)" the (3) goes to 1, and the bar flashes, thats good.. when i press "START(2)" the (3) goes to 45 and here should the bar stop flashing, because its above 10 now, but i dosent! So i made another buttom(7) that does nothing else than stopping the bars from flashing. Also i have a "Every day speed(6)" buttom, that puts the (3) to 45, but then the bar starts flashing? Heres my guess, When i press the (6) it counts (fast ofc.) to 45 starting with 1, that makes the bar flashing? like this "1-bar starts,2,3,4,5,6,....45" and then i need to turn i off again with the (7) buttom :/ same thing if i uses the (4) then the bar starts flashes no mater what.. Okay, here is what i want it to do... I want the red bar(5) to flash when the "wincc gauge control" getsto 1, or better below10 and start again when it gets above again... Ifit too hard to under stand i belive i can find a way toupload it some where.. Thanks. Kasper |
7/18/2006 2:56 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Hi Kasper You should use a Dynamic Dialog script to do this - very easy [:D] You do not say what version of WinCC you have. So I cannot post an example but here are the steps to do this manually : - Open the Properties Dialog window for the rectangle - Go to Flashing -> Flashing Background property - Right-click on the lightbulb in the Dynamic column and select Dynamic Dialog - Configure the expression to point to your tag - Set the Data Type to Analog and enter the relevant ranges I have attached a bitmap of my Dynamic Dialog script Hope this helps Salma Attachmentflashing.zip (262 Downloads) |
7/19/2006 9:19 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
I am glad you have it working [:D] Just disregard my previous post. |
Follow us on